您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: Laser Beam Analysis (26)

光束质量和斯特列尔比

There are several metrics used to describe the quality of a laser beam including the M2 factor, the beam parameter product, and power in the bucket

立即查看 添加到收藏夹

激光器谐振模

The length of a laser resonator determines the laser’s resonator modes, or the electric field distributions that cause a standing wave in the cavity.

立即查看 添加到收藏夹

了解并指定激光元件的激光损伤阈值(LIDT)

Laser induced damage threshold (LIDT) denotes the maximum laser fluence an optical component can withstand with an acceptable amount of risk.

立即查看 添加到收藏夹

激光扩束镜

Laser beam expanders are critical for reducing power density, minimizing beam diameter at a distance, and minimizing focused laser spot size.

立即查看 添加到收藏夹

高斯光束传播

Understanding Gaussian beam propagation is critical for understanding laser systems because many lasers are assumed to have Gaussian profiles.

立即查看 添加到收藏夹

激光损伤阈值测试

Testing laser induced damage threshold (LIDT) is not standardized, so understanding how your optics were tested is critical for predicting performance.

立即查看 添加到收藏夹

高功率光学镀膜的复杂情况

Want to know more about high-power optical coatings? Find out more about the importance, fabrication, and testing at Edmund Optics.

立即查看 添加到收藏夹

常用激光光学材料

Understanding the most commonly used laser optics materials will allow for easy navigation of EO’s wide selection of laser optics components.

立即查看 添加到收藏夹

高反射率镀膜

Highly reflective (HR) coatings are applied to optical components to minimize losses when reflecting lasers and other light sources.

立即查看 添加到收藏夹

表面损伤

Subsurface damage in optical components can lead to increased absorption and scatter, reducing system performance.

立即查看 添加到收藏夹

Coherent® 激光器选择指南

Compare Coherent Laser specifications with the Edmund Optics selection guide.

立即查看 添加到收藏夹

夹杂物和气泡的均匀性和散射

Inhomogeneity and scatter from inclusions and bubbles in optical components can lead to worse performance, especially in laser optics applications.

立即查看 添加到收藏夹

光束直径对激光损伤阈值的重要性

The diameter of a laser highly affects an optic’s laser induced damage (LIDT) as beam diameter directly impacts the probability of laser damage.

立即查看 添加到收藏夹

超快激光的激光损伤阈值

The short pulse durations of ultrafast lasers make them interact with optical components differently, impacting the optic’s laser damage threshold.

立即查看 添加到收藏夹

增透膜

Anti-reflection (AR) coatings are applied to optical components to increase throughput and reduce hazards caused by back-reflections.

立即查看 添加到收藏夹

LIDT 规范中的 不确定性

Laser induced damage threshold (LIDT) of optics is a statistical value influenced by defect density, the testing method, and fluctuations in the laser.

立即查看 添加到收藏夹

Liquid Lenses in Imaging

Liquid lenses have many features, are small in size, and adjust focus quickly to adapt to objects located at various working distances. Learn more at Edmund Optics.

立即查看 添加到收藏夹

非球面透镜不规则度与斯特列尔比

The Strehl ratio of an optical system is a comparison of its real performance with its diffraction-limited performance.

立即查看 添加到收藏夹

反射镜金属镀膜

Want to learn more about metallic mirror coatings? Find information about standard and custom metallic mirror coatings that are available at Edmund Optics.

立即查看 添加到收藏夹

光学基片的热力学性质

The thermal properties of optical substrates including the CTE, dn/dT, and thermal conductivity are critical for predicting real-world performance

立即查看 添加到收藏夹

光学镀膜简介

Optical coatings are used to influence the transmission, reflection, or polarization properties of an optical component.

立即查看 添加到收藏夹

激光光学计量

Metrology is critical for ensuring that optical components consistently meet their desired specifications, especially in laser applications.

立即查看 添加到收藏夹

使用柱面透镜时的其他考虑事项

Learn about specifications that should be considered when using cylinder lenses, including power axis wedge, plano axis wedge, and axial twist at Edmund Optics.

立即查看 添加到收藏夹

散射

Dispersion is the dependence of the phase velocity or phase delay of light on another parameter, such as wavelength, propagation mode, or polarization.

立即查看 添加到收藏夹

了解表面质量

The surface quality of optical components the scattering off of its surface, which is especially important in laser optics applications.

立即查看 添加到收藏夹

激光系统的关键参数

了解确保激光应用成功必须考虑的关键参数。将为这些参数建立通用术语。

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号